How to authenticate MIFARE Plus SE card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to authenticate MIFARE Plus SE card

4,715 次查看
liangjiahua1
Contributor I

Hi,

I use ISO 14443-3 protocol to send “Following authentication” command but get the error code 0x04 (It seems that it means “Block Number out of Range”). Please see below detail:

PCD send: 0x76 0x04 0x40 0x71 0xD6

PICC respond: 0x04

Note: “0x04 0x40” is the AES Sector Keys for Key A for sector 2, LSB first.

What is wrong with it?

0 项奖励
回复
3 回复数

3,656 次查看
xiongqinghua
Contributor I

I have the same question!!!

0 项奖励
回复

3,656 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

You have to request the export control version of NFC reader library from the docstore. Please refer to the following for details.

pastedImage_1.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,653 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Liang Jiahua,

We have documentation for this topic, but you have to request it from docstore.nxp.com. Please kindly refer to the attachment for more details.

Hope that helps,

Best regards,

Kan

0 项奖励
回复