How much power allowed to be consumed by the NFC Rx ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How much power allowed to be consumed by the NFC Rx ?

1,688件の閲覧回数
dkh
NXP Employee
NXP Employee

How much power allowed to be consumed by the NFC Rx ?

I am using Android phone and would like to power and communicate to external device.

0 件の賞賛
返信
1 返信

1,451件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Dennis,

Please provide more details to understand your question.

What do you mean with NFC Rx?

What is the external device you would like to communicate with?

I believe you are referring to taking energy from the NFC Field. The amount of power that can be consumed from the field depends on several factors, such as the field strength itself, the coupling coefficient between the Reader and Target antennas and the form factor of the antennas as well as the corresponding matching/tuning circuits. So because of these variants I would like to understand your question better.

Regards!

Jorge Gonzalez

0 件の賞賛
返信