How do I inject current in the RFID system to increase the range?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I inject current in the RFID system to increase the range?

1,428件の閲覧回数
mnfsoft
Contributor I

I have only the  MFRC522 I.C. with the default design as shown in the datasheet of the I.C. on page 81 but from my ANTENNA knowledge I know if you inject more current in the system I may extend the effective range to more than 50mm but I am not sure how to do this plus If I use active card I can achieve this but how since the I.C. is very sensitive with low power mode (very preferable) I do not want to damage the I.C. ??? where a max. range is very preferable (in the order of 100mm or more)

P.S. I have this circuit made by a Chinese manufacturer and marketed as ARDUINO equipment!

タグ(2)
0 件の賞賛
返信
1 返信

1,371件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

sorry, we don't have the information about how to inject current to increase the range.

0 件の賞賛
返信