How can I update my Firmware OM26630FSK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I update my Firmware OM26630FSK

Jump to solution
3,585 Views
lutzmüller
Contributor I

When I start NFC Cockpit I get:
[2018.02.03 15:39:48]:INFO:ServiceFactory:Generating Services for VCOM_RC663 @COM3
[2018.02.03 15:39:48]:ERROR:ServiceFactory:Invalid Interrupt Trigger Detected!!
[2018.02.03 15:39:48]:ERROR:ServiceFactory:m_bal.SetConfig(HalHwType,RC663) failed. Status=GENERIC,USE_CONDITION
[2018.02.03 15:39:48]:ERROR:ServiceFactory:generateServices(VCOM_RC663 @COM3) Failed with GENERIC,USE_CONDITION
[2018.02.03 15:39:48]:INFO:ServiceFactory:uC FW Version: NNC_uC_VCOM_01.01.00_20170130 (Compiled on Feb  2 2017 14:36:40)
[2018.02.03 15:39:48]:WARN:ServiceFactory:Please use the MicroController FW provided with this version of the GUI
[2018.02.03 15:39:48]:ERROR:ServiceFactory:SelectBalHalOsal(selected_board) Failed with GENERIC,USE_CONDITION
[2018.02.03 15:39:49]:WARN:UcVcomBalDelegate:Assuming Secondary FW Upgrade is supported

Tags (2)
0 Kudos
Reply
1 Solution
3,111 Views
phamsa
Contributor III

Hi,

You can update firmware from NFC Cockpit, right hand top there is tab named extra.  from there you can update, .bin file you can find in installation folder of NFC cockpit, during this process board need to be connected and also VCOM drivers installed.

for VCOM drivers you can search in same NFC Cockpit installation folder.

hope this helps

Thank you

View solution in original post

0 Kudos
Reply
3 Replies
3,112 Views
phamsa
Contributor III

Hi,

You can update firmware from NFC Cockpit, right hand top there is tab named extra.  from there you can update, .bin file you can find in installation folder of NFC cockpit, during this process board need to be connected and also VCOM drivers installed.

for VCOM drivers you can search in same NFC Cockpit installation folder.

hope this helps

Thank you

0 Kudos
Reply
3,111 Views
rutger
Contributor I

Hi,

I've tried just about everything that comes to mind, but keep getting the same behavior, this is what the log window contains. The instructions you gave don't seem to work and the drivers have been installed. Please advise!

[2018.04.22 10:47:31]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:47:32]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:47:54]:FATAL_ERROR:BoardConnectService:Error closing COM Port The device is not connected.

[2018.04.22 10:48:06]:INFO:ServiceFactory:Generating Services for VCOM_RC663 @\\.\COM14
[2018.04.22 10:48:06]:ERROR:ServiceFactory:Invalid Interrupt Trigger Detected!!
[2018.04.22 10:48:06]:ERROR:ServiceFactory:m_bal.SetConfig(HalHwType,RC663) failed. Status=GENERIC,USE_CONDITION
[2018.04.22 10:48:06]:ERROR:ServiceFactory:generateServices(VCOM_RC663 @\\.\COM14) Failed with GENERIC,USE_CONDITION
[2018.04.22 10:48:06]:INFO:ServiceFactory:uC FW Version: NNC_uC_VCOM_01.01.00_20170130 (Compiled on Feb 2 2017 14:36:40)
[2018.04.22 10:48:06]:WARN:ServiceFactory:Please use the MicroController FW provided with this version of the GUI
[2018.04.22 10:48:06]:WARN:UcVcomBalDelegate:Assuming Secondary FW Upgrade is supported
[2018.04.22 10:48:06]:ERROR:ServiceFactory:SelectBalHalOsal(selected_board) Failed with GENERIC,USE_CONDITION
[2018.04.22 10:48:47]:INFO:SecondaryFirmwareService_UCBal:Sending command to enter FW Upgrade Mode
[2018.04.22 10:48:47]:INFO:UcVcomBalDelegate:Sleeping for 1ms to entry into FW Upgrade Mode
[2018.04.22 10:48:48]:WARN:ServiceBroker:SecondaryFirmwareViewModel is Re-acquiring SecondaryFirmware
[2018.04.22 10:48:48]:WARN:ServiceBroker:SecondaryFirmwareViewModel is Re-acquiring BoardConnect
[2018.04.22 10:48:48]:ERROR:SecondaryFirmwareService_UCBal:SerialPort.IsOpen
[2018.04.22 10:48:48]:WARN:SecondaryFirmwareViewModel:Please close COM Port and open again.
[2018.04.22 10:48:53]:INFO:ServiceFactory:Generating Services for VCOM_BootLoader @\\.\COM14
[2018.04.22 10:48:55]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:48:56]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:48:57]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:48:58]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:48:58]:WARN:ServiceFactory:Please use the MicroController FW provided with this version of the GUI
[2018.04.22 10:50:16]:INFO:ServiceFactory:Generating Services for VCOM_BootLoader @\\.\COM14
[2018.04.22 10:50:17]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:50:19]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:50:20]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:50:21]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while reading from COM14
[2018.04.22 10:50:21]:WARN:ServiceFactory:Please use the MicroController FW provided with this version of the GUI

0 Kudos
Reply
3,111 Views
olegtcaregorodt
Contributor II

Hi,

I'm hitting the same issue with NFC Cockpit v4.7.0.0

Under the tab "extra" there's only a tab "Secondary FW". I've found a folder called C:\nxp\NxpNfcCockpit_v4.7.0.0\firmware\Secondary_RC663, which looks like the most relevant one. The readme there says:

Binaries for LPC1769 :

RC663 Board Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin: (For IDE)

- Reference secondary Firmware to be run on LPC1769 on the given Board - This file should be loaded through Secondary FW Upload feature of the GUI on LP1769 - This reference applicaiton implement 3 Minimal RTOS Tasks to perform RF On/OFF and ON-OFF - This applicaiton implements EMVCo Loop Back

BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin: (For Debuggers)

- Binary file that has already stacked Boot loader from address 0x0000 onwards and Upper Secondary Application at address 0x4000. This file can be used to flash on LPC1769 as a single binary from address 0x0000 onwards using relevant Debuggers/Flash Programmers.

extra/phRfOnOff_Secondary.bin:

extra/BootLoader_And_phRfOnOff_Secondary.bin: - Similar to Nfcrdlib_SimplifiedAPI_EMVCo_Secondary, but a minimal firmware that can be used to just perform RF On/RF Off for testing.

which one is relevant for the intended out-of-the-box functionality?

Thanks,

Oleg

0 Kudos
Reply