How can I read Iphone UID or any data using CLRC663 Reader?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I read Iphone UID or any data using CLRC663 Reader?

1,800 Views
islambedair2
Contributor I

I Have CLRC663 plus NFC Frontend Development Kit for Access Management Application and I want to read iPhone UID or Any message form it for access control application

Labels (1)
0 Kudos
Reply
1 Reply

1,756 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

The CRLC663 supports

Read / Write mode

  • ISO/IEC 14443A (NTAG® and MIFARE® product family)
  • ISO/IEC 14443B
  • JIS X 6319-4 (comparable with FeliCa1 scheme)
  • ISO/IEC 15693 (ICODE® SLIX, SLIX2, DNA)
  • ISO/IEC 18000-3 mode 3/ EPC Class 1 HF (ICODE® ILT)


Peer to Peer mode

  • Passive Initiator according to ISO/IEC 14443A (106kbit/ and FeliCa (212 and 424kbit/s)

Still, you will need to check the documentation of the phone and the options that are enabled for the developers to work with.

Regards,

Estephania

0 Kudos
Reply