How can I read Iphone UID or any data using CLRC663 Reader?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I read Iphone UID or any data using CLRC663 Reader?

1,793件の閲覧回数
islambedair2
Contributor I

I Have CLRC663 plus NFC Frontend Development Kit for Access Management Application and I want to read iPhone UID or Any message form it for access control application

ラベル(1)
0 件の賞賛
返信
1 返信

1,749件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

The CRLC663 supports

Read / Write mode

  • ISO/IEC 14443A (NTAG® and MIFARE® product family)
  • ISO/IEC 14443B
  • JIS X 6319-4 (comparable with FeliCa1 scheme)
  • ISO/IEC 15693 (ICODE® SLIX, SLIX2, DNA)
  • ISO/IEC 18000-3 mode 3/ EPC Class 1 HF (ICODE® ILT)


Peer to Peer mode

  • Passive Initiator according to ISO/IEC 14443A (106kbit/ and FeliCa (212 and 424kbit/s)

Still, you will need to check the documentation of the phone and the options that are enabled for the developers to work with.

Regards,

Estephania

0 件の賞賛
返信