HTRC110

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HTRC110

2,392件の閲覧回数
avskulkin
Contributor I

whats the difference between HTRC11001T/02EE and HTRC11001T/03EE?

ラベル(1)
0 件の賞賛
返信
1 返信

2,387件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello.

The difference of the both part numbers is packing.HTRC11001T/02EE is TUBE-Bulk Pack.HTRC11001T/03EE is REEL-Reel 13" Q1/T1.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信