HTRC110

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HTRC110

2,395 Views
avskulkin
Contributor I

whats the difference between HTRC11001T/02EE and HTRC11001T/03EE?

Labels (1)
0 Kudos
Reply
1 Reply

2,390 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello.

The difference of the both part numbers is packing.HTRC11001T/02EE is TUBE-Bulk Pack.HTRC11001T/03EE is REEL-Reel 13" Q1/T1.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply