HF Tags

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HF Tags

1,672 Views
mohemed_aslan
Contributor I
I have a project and i need Tags for it. i will explain in bellow. please help me and introduce the best product.
I am using  V680S-HMD64-EIP Omron reader/writer. I know omron have several tags model but they are with read and write with more cycle time. we have some carton that only use for 10 time therefore we need tags with low read / write cycle time because after 10 time we will throw away carton with tags. what is suggestion for our project? we need cheap tags. 
I'm waiting to your answer. it is very force for me.
0 Kudos
Reply
1 Reply

1,564 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear mohemed aslan, 

please check the following tags:

ProductsStandardUser memory [bit]
ICODE DNA
SL2S6002FUD
ISO
18000-3M1
2016-
ICODE SLIX 2
SL2S2602
ISO
18000-3M1
2528
ICODE SLIX
SL2S2002 / SL2S2102
ISO
18000-3M1
896
ICODE SLIX-L
SL2S5002 / SL2S5102
ISO
18000-3M1
256
ICODE SLIX-S
SL2S5302 / SL2S5402
ISO
18000-3M1
1280

please check this tags all of them have data transfer: up to 53 kbit/s. the most complete of this is the slix S  but if you do not need the amount of features please check the slix. in this link you can found the ICODE®|NXP  family and you can compare their features.

BR

Jonathan

0 Kudos
Reply