HChange security level 0 on mifare plus with APDU command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HChange security level 0 on mifare plus with APDU command

2,454 Views
mygodess
Contributor I

We are using nxp mifare plus in mass production.

When we want to use it as mifare classic, the secutiry level should be changed NXP said.

There is a tool named RFID Discover to change the mifare security level 0 data  but it is not designed for mass production. 

I used it for pre production but I need to change the security block in mass production.

Is there the way to change it with APDU commands? 

 

0 Kudos
Reply
5 Replies

2,354 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @mygodess 

Ok, if you have an NDA, then you need to send email support.docstore@nxp.com  to request access to these documents.

KellyLi_0-1724766754027.png

 

0 Kudos
Reply

2,421 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @mygodess 

Yes, RFID Discover can do what you want, but it's not suitable for mass production. However, the design resource you want are the security documents, and you need to sign an NDA with NXP to have access. 

so please establish an NDA with NXP by going to  https://www.nxp.com/support/support:SUPPORTHOME and select "Request an NDA"

 

KellyLi_0-1724649551329.png

 

0 Kudos
Reply

2,279 Views
mygodess
Contributor I
I got the Card Test Framework and trying to change mifare Security Level. I still have some problem to write Perso. There is the example to do similar one with Desfire but it does not help that much to do with Mifare Plus. Is there some example for Mifare plus? Maybe there is tome problem to authenticate.
0 Kudos
Reply

2,371 Views
mygodess
Contributor I

I’m working in a company in Korea and we already have NDA. 

Should I get get another one? 

And I want to get a pdf document name also.

There are lots of documents and it is very hard to find the document I want. 

0 Kudos
Reply

2,253 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @mygodess 

Have you got the two documents mentioned above?

KellyLi_0-1725436798161.png

 

0 Kudos
Reply