Gerber file usage - AN11276

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gerber file usage - AN11276

ソリューションへジャンプ
4,388件の閲覧回数
EthanMathew25
Contributor III

Hi, 
Can I use the Gerber files provided along with NXP NTAG I2C NFC IC as it is without making any modifications to them ?
Can I use them on different substrates ? how much performance degrade will be there ? How to overcome those ? 

0 件の賞賛
返信
1 解決策
4,261件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello,

Ok, it should be fine. 

Anyhow, once you produce the antennas, it is recommended to measure them with the help of the VNA and potentially tune the tag by a parallel capacitor as shown below. 

Tomas_Parizek_0-1707201529860.png

BR

Tomas 

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,323件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello EthanMathew25, 

Do you mean the following files located in AN11276?

Tomas_Parizek_0-1706606231071.png

BR 

Tomas

0 件の賞賛
返信
4,311件の閲覧回数
EthanMathew25
Contributor III
yess! those files...
can I use them on any substrate or do I have to make any changes?
0 件の賞賛
返信
4,278件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello EthanMathew25, 

What substrate are you planning to use? 

Yes, as the antenna turns are only on one layer, the different substrates should not have any major impact. 

We typically use a standard FR4 or Flex. 

BR

Tomas 

 

4,271件の閲覧回数
EthanMathew25
Contributor III
Polyimide substrate
0 件の賞賛
返信
4,262件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello,

Ok, it should be fine. 

Anyhow, once you produce the antennas, it is recommended to measure them with the help of the VNA and potentially tune the tag by a parallel capacitor as shown below. 

Tomas_Parizek_0-1707201529860.png

BR

Tomas 

 

0 件の賞賛
返信
4,361件の閲覧回数
EthanMathew25
Contributor III

@Tomas_Parizek Help me out...

0 件の賞賛
返信