Faced an issue while executing an ECP example from "NxpNfcRdLib_Linux_v07.09.00_ECP"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Faced an issue while executing an ECP example from "NxpNfcRdLib_Linux_v07.09.00_ECP"

1,684 Views
IXM
Contributor I

Hello All, 

We want to implement a APPLE VAS protocol on CLRC66303 reader IC. For that we have a ECP supported latest library from NXP with apple certification. I've added a digital PASS for demo in the apple wallet. But whenever I tried to tap on reader pass is detected as a "Desfire", Gives me a random UID and type of the same, after execution of the ECP example. Does not get any response after VAS command execution. It gives me an error code 0x201, It means card is not in range. 

Also reader is not able to perform PICC level authentication, It gives an error code of 0x2006, Which means "Received response violates the protocol". 

I didn't understand this, Please help me for the same. Is there any key issue ? Or I miss something ?

Note(s):

1. Find the link from which I have added a digital pass in apple wallet : https://help.passkit.com/en/articles/4430727-enabling-and-using-nfc-passes

2. NXP library version :  NxpNfcRdLib_Linux_v07.09.00_ECP

Thanks.

0 Kudos
Reply
1 Reply

1,668 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @IXM 

 

ECP feature is secured under NDA (Non-Disclosure-Agreement).  I would suggest you contact the person who sent you this package for help.

 

Regards

Danie

,

 

0 Kudos
Reply