ExploreNFC P2P sending file to Android device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ExploreNFC P2P sending file to Android device

1,687件の閲覧回数
ivanrodriguez
Contributor I

Hi all:

I just bought an ExploreNFC board. I would like to send an small file from the nfc board to Android application. I found on the Internet the P2P-SNEP_clientPUT project and when I run it, I didn't receive anything on the phone.

Please note that I have an Android application running, with NFC enable and based on NFC Basics | Android Developers 

タグ(3)
0 件の賞賛
返信
1 返信

1,426件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Ivan,

This initial P2P example is discontinued because of instabilities. The NXP recommendation is to use the latest Nxp NFC  Reader Library package available for Linux (can be downloaded from here the NFC Reader Library web page).

The package demonstrates full NFC functionalities (including P2P SNEP communication and by default is running on Raspberry Pi toether with EXPLORE-NFC board.

Refer to AN11802 for more details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信