Excessive Current for LPCD mode (CLRC663)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Excessive Current for LPCD mode (CLRC663)

1,638件の閲覧回数
jr_hernandez
Contributor II

Hello,

I am assessing the CLRC663/plus for a battery-powered application. I am testing the LPCD mode with the evaluation kit (OM26630FDK -> CLEV6630B) and the current consumption is much higher than expected.

I am using 1000ms (as ON time) and 2 us (as OFF time). But I have tested also other timing configurations.

Current measured in VDD + TVDD (accross the jumpers) @ 3,3Vdc is no lesser than 200 uA.

¿Is this the typical current for LPCD?

¿Is there any missing setting?

In the datasheet the LPCD current is supposed to be between 3.3 uA and 12 uA.

Could you please help on finding the trick for using LPCD at rated datasheet currents: 3-12 uA.

Regards, Ramón.

ラベル(1)
0 件の賞賛
返信
1 返信

1,600件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Please remember that on the evaluation board we have a lot of other devices connected that can be affecting the measurement.

Also, I do not know if you already check the recommendation on the following application note

https://www.nxp.com/docs/en/application-note/AN11783.pdf 

I hope this will help you

Regards

Vicente

0 件の賞賛
返信