Encoding NTAG424 with mobile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encoding NTAG424 with mobile

1,654 Views
Lowos
Contributor I

Dear NXP community,

We have a point, we want to encode all our NTAG424 with mobiles and without the use of a computer.

So because of AES, it seems that no all the mobiles can do that but basically do you know an mobile app that could do that ? (Famous ones are NFC Tools and TagWriter from NXP?).

Best and thanks for your answers.

Louis

0 Kudos
Reply
2 Replies

1,621 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Lowos,

Hope you are doing well.

TagWriter mobile app provides the means to perform read/write/erase operations, use mirroring features, protect tags, do a mass encoding, backup and import the dataset. These operations are described in the TagWriter User Manual.

Any additional requirements would require the customer to develop a custom application implementing such functionality based on the documentation that is available for the NTAG 424.

Regards,
Eduardo.

0 Kudos
Reply

1,647 Views
Lowos
Contributor I

Mobile phones*

0 Kudos
Reply