ECP NFC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECP NFC

6,013 Views
ralfschmale
Contributor I
Hello
 
We use in our application the CLRC663 Reader for NFC. Our customer request a functionality ECP.
is it possible do this ECP only with the PC7150X or is it also possible via SW with the CLRC663?
 

PN7150X: High-performance NFC controller IC with support for Apple Enhanced Contactless Polling (ECP)

 
Best regards
 
0 Kudos
Reply
3 Replies

5,487 Views
janulo
Contributor III

Hi IvanRuiz , I'm also interested in support of ECP via software, this time on PN5180. So it it possible to support ECP on PN5180? Thanks for response.


Regards

Jan

0 Kudos
Reply

5,487 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

ECP is currently implemented in PN7150X. for further questions regarding ECP in this or other devices, please contact apple tech support.

Thank you for your comprehension.

Best regards,

Ivan.

0 Kudos
Reply

5,487 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

An update was made to your question via case.

Regards,

Ivan.

0 Kudos
Reply