Does the RC663 chip have RSSI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the RC663 chip have RSSI?

3,743件の閲覧回数
m4416202
Contributor I

Hello

       We use the CLRC663 blueboard to develop new product.But our customer wish to know the value of "RSSI". So we want know where can we get the RSSI's value of RC663?Or which  register ?

thanks

0 件の賞賛
返信
4 返答(返信)

3,232件の閲覧回数
jhernandez
Contributor II

Thanks for info IvanRuiz‌

0 件の賞賛
返信

3,232件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello,

In a normal radio communication, we have one device as Tx and other as Rx. The carrier is transmitted by the Tx and the Rx can measure the RSSI.

In NFC, the Rx (our Reader) transmits the carrier itself while the Tx (the card/tag) just "loads" the field. So, which radio strength you would like to measure?

The question might be about the strength of the coupling, e.g. you could measure the strength of the subcarrier or you could measure the loading effect as a kind of strength ... or anything else?

Regards,

Isaac

0 件の賞賛
返信

3,232件の閲覧回数
jhernandez
Contributor II

About the RSSI, we are developing a reader with several antennas (we use a multiplexer). Is there any parameter that can measure with the clrc663 to be able to discern if a tag is closer to one antenna than another?

Thank you!

0 件の賞賛
返信

3,232件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

It is not possible to know the distance at which the tag is because of the explained above. Unfortunately DPC feature is not available on this board which allows to control the transmitter current and therefore the field strength depending on loading and detuning conditions.

DPC feature is available in PN5180 and PN7462.

have a good day.

Regards,

Ivan.