Does the RC663 chip have RSSI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the RC663 chip have RSSI?

3,671 Views
m4416202
Contributor I

Hello

       We use the CLRC663 blueboard to develop new product.But our customer wish to know the value of "RSSI". So we want know where can we get the RSSI's value of RC663?Or which  register ?

thanks

0 Kudos
Reply
4 Replies

3,160 Views
jhernandez
Contributor II

Thanks for info IvanRuiz

0 Kudos
Reply

3,160 Views
isaacavila
NXP Employee
NXP Employee

Hello,

In a normal radio communication, we have one device as Tx and other as Rx. The carrier is transmitted by the Tx and the Rx can measure the RSSI.

In NFC, the Rx (our Reader) transmits the carrier itself while the Tx (the card/tag) just "loads" the field. So, which radio strength you would like to measure?

The question might be about the strength of the coupling, e.g. you could measure the strength of the subcarrier or you could measure the loading effect as a kind of strength ... or anything else?

Regards,

Isaac

0 Kudos
Reply

3,160 Views
jhernandez
Contributor II

About the RSSI, we are developing a reader with several antennas (we use a multiplexer). Is there any parameter that can measure with the clrc663 to be able to discern if a tag is closer to one antenna than another?

Thank you!

0 Kudos
Reply

3,160 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

It is not possible to know the distance at which the tag is because of the explained above. Unfortunately DPC feature is not available on this board which allows to control the transmitter current and therefore the field strength depending on loading and detuning conditions.

DPC feature is available in PN5180 and PN7462.

have a good day.

Regards,

Ivan.