Detecting iOS phone using PN7642

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Detecting iOS phone using PN7642

2,659件の閲覧回数
Prajna
Contributor I

Hi,

I was looking into discovery loop to detect and print the UID and SAK bytes of different types of cards. I also wanted to check it with the smartphone. When i place an android phone i am able to see UID and SAK and it prints out as a type 4A credential. But when i place apple phone, i don't see it printing anything. I have even tried using Nfrcrdlib_SimplifiedAPI_ISO_Freertos example too but it was also not able to detect the presence of iOS device.

My question is, is it possible to print or atleast detect the presence of apple phone when it is brought near the PN7642 reader. If it is possible can someone tell me what changes should be made.

 

Thanks

タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,602件の閲覧回数
Prajna
Contributor I

So, there is no way to just detect and print the UID of iphone when it is brought closer to the reader?

 

0 件の賞賛
返信

2,591件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello!

Unfortunately, it is necessary to implement the ECP support in the Reader to do so.

Best Regards,
Fabian
0 件の賞賛
返信

2,552件の閲覧回数
Prajna
Contributor I
I see that there is ECP freertos example, will this be able to detect iPhone?
0 件の賞賛
返信

2,531件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

This is correct but, please keep in mind that the access to this software has to be done through our Distributors since it is a very restricted topic and, I don't have these information.

Best Regards,
Fabian
0 件の賞賛
返信

2,622件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello, my name is Fabian, I've been assigned to support your case.

Thank you for your interest in our products.

The reason why the PN7642 isn't able to read the iPhone is because, iPhone doesn't emulate a type 4 tag. It can emulate cards but, through a proprietary protocol.

Our Reader do support this protocol but, in order to get access it is required to contact your Distributor since this is a very restricted software.

Unfortunately, the PN7642 won't detect your iPhone if your software doesn't support ECP even if you are using a emulation of a card. i.e. Transport Card or ApplePay.

Best Regards,
Fabian
0 件の賞賛
返信