Current consumption NT3H211 EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Current consumption NT3H211 EEPROM

2,360件の閲覧回数
dominik_neeser
Contributor I

Dear NXP Support,

 

I am looking for the nominal current consumptions of the NXP tag NT3H2111_2211

In chapter 13.1 “13.1 Electrical characteristics” of the datasheet I can only find a current consumption referring to I2C.

 

However I am interested in the current consumption for writing data to the internal Tag EEPROM via I2C (without giving any NFC field).

3 返答(返信)

2,203件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please see below information from the internal team:

NTAG I²C plus consumes 185µ[email protected] when I²C in Stand-by / Active state (for v1 version that value is 155µA) – this is with considered leakage on SDA, SCL lines (10µA).

 

Average during EE Read                  =  like standby
Max during EE Read Access            = +60 µA
Average during EE Write                  = +30 µA
Max during EE Write Access            = +160 µA
Average during I2C Register Read   = +10 µA
Average during I2C Register Write   = +10 µA

 

“0 power consumption” may be achieved by:

 Try to turn OFF NTAG's Vcc until:

  • I²C communication is needed
  • Usage of SRAM is needed

 

Detect RF activity (MCU “knows” RF field is present)

  • Vout goes high when tag is exposed to RF field
  • Configure FD pin to go low on RF activity for (open drain – needs pullup)

 

Recommendations:

  • FD pin pull-up above 1kOhm
  • General I²C BUS pull-up for each line SDA, SCL (depends on bus load, but usually around 1k – 10kOhm)
  • Capacitor in range 100nF – 200nF from Vout to GND
  • NTAG's SDA, SCL, Vcc controlled by MCU

Regards,

Ivan.

2,203件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

I am currently waiting for internal confirmation about your request. I will come back asap.

Regards,

Ivan.

0 件の賞賛
返信

2,203件の閲覧回数
dominik_neeser
Contributor I

Hello Ivan,

is there any conformation already available?

Thanks in advance,

Dominik

0 件の賞賛
返信