Confirmation of PN7362 protocol issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Confirmation of PN7362 protocol issues

772 次查看
Karyliu
Contributor II

Hi NXP,

There is a diagram in PN7150datasheet that reads and writes Sony FeliCa according to ISO/IEC18092 standard. This illustration is not available on PN7362.

But in the selection table, it is written that PN7362 supports ISO18092 and FeliCa. It is uncertain whether PN73262 follows ISO18092 when reading and writing FeliCa cards on the USB CCID interface?

Thank you.

0 项奖励
回复
1 回复

711 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi

Unfortunately,we do not provide complete support for Felica cards. Our reader library is capable of detecting Felica cards and activate them, all additional tags' operations shall be implemented by customers, in case you require more information about Felica's commands, please contact Sony support.

 

 

Regards

Daniel

0 项奖励
回复