Complex Logic for Discovery Loop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Complex Logic for Discovery Loop

1,589件の閲覧回数
aceviker
Contributor I

Hi, I need to implement a loop where a Layer 4 Type A card with a specific application is selected and any other type of card is ignored. Even if multiple card types or multiple Layer 4 Type A cards are on the reader the reader must select with the Layer 4 Type A with the correct application.

How can i achive this with the discovery loop. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,508件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

The discovery loop will only poll for types, the switching to Layer 4 and selection of the correct Tag with specific information shall be carried out on the application side.

Best regards,

Ivan.

0 件の賞賛
返信