Change EEPROM user_ee.bin for PN7462

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change EEPROM user_ee.bin for PN7462

1,961 Views
n_biniossek
Contributor I

Hi all,

I currently try to update the EEPROM memory according to our needed AGC and Gain values. Unfortunately, I’m only able to update the values in the NXP NFC Cockpit software whenever I use the default software for the PNEV7462. Therefore, I modified the basic EEPROM.bin file according to my needs and saved it. After that I flash both parts the modified EEPROM.bin file and our normal software at our product. Unfortunately, the software crashed every time according to the different EEPROM firmware numbers and because phCfg_EE.c and phCfg_EE.h was not updated.

I already read the „EEPROM Management of PN746X and PN736X“ (UM10948)  but I’m not able to change the parameters in the configuration xml files according to our needs (like with the NFC Cockpit). Is there any kind of description how to change the xml configuration files to change the AGC and gain parameters? Otherwise you please provide a simple example how to do it.

Many thanks in advance! I’m looking forward to your answer.

Best,

Nik

0 Kudos
Reply
1 Reply

1,685 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Which parameters did you change in NFC Cockpit? So we can relate them to the XML file and see what is the problem. 

 

Just to be sure; the correct way would be to change the values within the XML file and execute the bat file which will generate the .bin as well as the phCfg_EE.c and phCfg_EE.h.

Regards,

Ivan.

0 Kudos
Reply