How to let CLRC663 board run without debug mode in MCUXpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to let CLRC663 board run without debug mode in MCUXpresso IDE

1,290 次查看
albertsung
Contributor I

Hi All,

I have the CLRC663 development kit (OM26630FDK) and it can work with the example codes in MCUXpresso IDE.

But if I disconnect the LPC-Link or if I only do the flash programming without debug mode in MCUXpresso IDE,

then the CLRC663 looks not working.

It seems it only can run with debug mode. Is there any method to run without debug mode ?

Best Regards,

Albert

 

标记 (3)
0 项奖励
回复
1 回复

1,081 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

What do you mean by not working? Do you have an error or something? which example you are using?  Could you please provide more details ? 

Regards

0 项奖励
回复