Certification for PN532

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Certification for PN532

4,360 Views
vaibhavchanana
Contributor I

My company has developed a product using PN532 chip and is now looking to get it certified (FCC and CE).

According to our research we need to change the following parameters :

  1. Channel Selection
  2. Continuous Transmission
  3. Bit Rate Selection
  4. Power Selection

I read the datasheet could not find a way to change these parameters. Can anyone help me ?

Thanks

Labels (2)
0 Kudos
Reply
2 Replies

4,281 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

The information about the commands is available in the following App Note: https://www.nxp.com/docs/en/nxp/application-notes/AN133910.pdf 

Please note that this is all the information we have at our reach since this device is not recommended for new designs. Thank you for your comprehension.

BR,

Ivan.

0 Kudos
Reply

4,273 Views
xt
Contributor I

is the PN532 allowed in the US? was also planning to design an RFID reader based on PN532 for door access but based on our research, 902~928MHz is the allowed frequency in the US. can PN532 is still be used which operates at 13.56MHz?

0 Kudos
Reply