Certification for PN532

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Certification for PN532

4,330件の閲覧回数
vaibhavchanana
Contributor I

My company has developed a product using PN532 chip and is now looking to get it certified (FCC and CE).

According to our research we need to change the following parameters :

  1. Channel Selection
  2. Continuous Transmission
  3. Bit Rate Selection
  4. Power Selection

I read the datasheet could not find a way to change these parameters. Can anyone help me ?

Thanks

ラベル(2)
タグ(5)
0 件の賞賛
返信
2 返答(返信)

4,251件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

The information about the commands is available in the following App Note: https://www.nxp.com/docs/en/nxp/application-notes/AN133910.pdf 

Please note that this is all the information we have at our reach since this device is not recommended for new designs. Thank you for your comprehension.

BR,

Ivan.

0 件の賞賛
返信

4,243件の閲覧回数
xt
Contributor I

is the PN532 allowed in the US? was also planning to design an RFID reader based on PN532 for door access but based on our research, 902~928MHz is the allowed frequency in the US. can PN532 is still be used which operates at 13.56MHz?

0 件の賞賛
返信