Cannot write to ISO15693 NFC tags using CLEV663 Development board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot write to ISO15693 NFC tags using CLEV663 Development board

2,215 次查看
software_memo
Contributor II

Hi,

I have a few Tag-It NFC cards (using ISO15693) from Texas instruments which were encoded by another manufacturer. I would like to use the same cards in parallel for my application too. To do this, I will require to write to some sectors of the NFC card memory. 

My setup consists of a CLEV663 board which is controller by the NXP NFC Cockpit v5.9 and a few Tag-It cards. 

I can perform all the read operations but I cannot write to NFC cards. Below is a list of the commands I executed and the response from the card;

Get System Information: Command: 0x2B, Flags: 0x12, Response: : SUCCESS, Data: 0F6B8AE52A000007E000003F038B

Get Multiple Block Security Status Blocks 0 and 1: Command: 0x2C0001, Flags: 0x12 Response: SUCCESS, Data: 0000

Read Block 1: Command: 0x2001, Flags: 0x12, Response: 00000000

Write Block 1 with data 0x33221100: Command: 0x210100112233, Flags: 0x52, Response: ERROR:RFProtocolType15693Service:Perform15693DataExchangeFailed: PAL_SLI15693,ISO15693

Even though the block security is not set, I cannot write to it. Can somebody please help?

0 项奖励
回复
1 回复

2,207 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Actually Cockpit is designed for hardware test purpose, and usually used for the antenna design and optimization, and we provide NFC reader library for custom application, this library includes the example for  ISO15693 as the link.

URL:https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NF....

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复