CT & CLIF Card Operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CT & CLIF Card Operation

3,246件の閲覧回数
sachin_singh
Fresh Out Contributor

Hi All,

I am working on the PN7462AU card reader with Evaluation kit using PN7462AU-FW_v05.07.01_Full firmware file with "phExCcid" example. Which is for Contact and Contact-less cards detection.

I need to perform the operation on both card when both are present at same time. But yes only one card get the command fired by the user respectlivily.

For example say that, Card reader has both the card Contact and contact-less card present at the same time. When user need to fire command for contact card then it should received by contact card similarly for the contact-less also. (For Contact-less card - MIFARE CLASSIC 1k and contact card - SAM CARD).

In short I need to perform the operation on both cards (contact and contact-less cards) but one at a time in presence to two cards - contact and contact-less cards.

So, Please kindly guide to achieve these functionality for two card operation on PN7462AU.

If possible then also share the API/data/document/any example related to it.

Your all the support & response are highly appreciative.

Looking forward for the supports.

Regards

0 件の賞賛
返信
2 返答(返信)

3,036件の閲覧回数
hglanzer
Contributor I

hi,

having the same problem as describe by 'sachin_singh'. could you elaborate how to solve this?

thx in advance

hari

0 件の賞賛
返信

3,162件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

A reply was already made to your case.

BR,

Ivan.

0 件の賞賛
返信