CRLC663, how to write data to tag

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CRLC663, how to write data to tag

1,037 次查看
Elly
Contributor I

Hello, 

I faced a problem to get response when writing data to tag. 

Tag communication uses ISO/IEC 15639 and CLRC663 chipset. 

Tag UID and reading single block(0x20 tag command) works well. However, there is no response for writing single block (0x21 tag command). 

There is no response (no Rx IRQ, no Err IRQ) when writing data to tag. 

Even if the response is not received, if I read the tag, the data is written correctly. 

Please let me know how can I resolve it? 

  • RFID Chipset: CLRC663
  • Host interface : RS232
  • RFID Tag Communication Protocol: ISO15693
  • Steps to write data : Loading protocol already done. 
    : Step1  Turns on RF
    : Step2.  Clear IRQ0  
    : Step3. Save packet to FIFO - 0x42(flag), 0x21(command), 0x00(block number), 0x01, 0x02, 0x03, 0x04 
    : Step 4. Execute transceiver
    : Step 5. Wait response (IRQ0) 
1 回复

812 次查看
ypearson
Contributor I
I got exactly the same issue, was there a solution to this?
0 项奖励
回复