CLRC663 INT Pull Up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 INT Pull Up

2,351 Views
MikeBrennan
NXP Employee
NXP Employee

Does the CLRC663 require a pull up resistor on the IRQ output pin or can it drive a uController input without the need of a pull up?

Labels (1)
0 Kudos
Reply
1 Reply

2,190 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Michael,

   IRQ pin doesn't need to be pulled up!  it's driver capability is enough.


Have a great day,
TIC   Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply