CLRC663 INT Pull Up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663 INT Pull Up

2,353件の閲覧回数
MikeBrennan
NXP Employee
NXP Employee

Does the CLRC663 require a pull up resistor on the IRQ output pin or can it drive a uController input without the need of a pull up?

ラベル(1)
0 件の賞賛
返信
1 返信

2,192件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Michael,

   IRQ pin doesn't need to be pulled up!  it's driver capability is enough.


Have a great day,
TIC   Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信