CLRC663 Antenna Layout review

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663 Antenna Layout review

4,869件の閲覧回数
nxf58908
NXP Employee
NXP Employee

Hello Team

Customer : Renu Electronics

Project : SMART DOOR LOCK ACCESS 

Hello Team,

Customer has designed Layout for NFC Antenna and wants to get it reviewed for any suggestion/recommendation.

 

Design Description:

CLRC663 & antenna are on two different boards. Two boards are connected through bergstrip. Separate bergstrip for Capacitive touch key IO's & RFID antenna connections.

 

  • Board 1 - MKL26Z256VLH4 MCU & CLRC66303HN & its matching circuit
  • Board 2 - Capacitive touch Keys - 12nos & RFID antenna pattern
  • We have used NXP tool to design the antenna pattern.

 

We need your review comments on -

 

  • Antenna pattern layout we designed on board

I am attaching Schematic and Layout PDFs along with GERBER files as well.

 

Thanks

Madhur

0 件の賞賛
返信
1 返信

4,863件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Generally, we can  review schematic(you can provide the schematic for it), as for PCB  - alas  - we do not have enough resources for it. The problem is that review of any PCB design  requires much time by an engineer, who has experience with PCB design. As has been mentioned, our support team has no resources for it. Sorry for the inconvenience may cause.

There is the application note for the customer can refer to it.

URL:https://www.nxp.com/docs/en/application-note/AN12334.pdf.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------


   

 

0 件の賞賛
返信