CLRC663-02 and CLRC663-03 INT Pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663-02 and CLRC663-03 INT Pin

2,133件の閲覧回数
MikeBrennan
NXP Employee
NXP Employee

I just wanted to confirm that there is no changes between the two revisions on the functionality of the INT pin?


Thanks,
Mike

ラベル(1)
0 件の賞賛
返信
1 返信

1,972件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Michael,

   Their INT (IRQ) functions are same.


Have a great day,
TIC  weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信