CLEV6630B not recognized by usb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLEV6630B not recognized by usb

1,851 Views
wegelinj
Contributor I

I have a CLEV6630B and it seems to be in a stuck or looped state, it will not connect or is recognized by my computers USB port any longer. Is there something I can try?

Tags (1)
0 Kudos
Reply
1 Reply

1,724 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Jackson,

Did you program the board with correct firmware? If you use cockpit with it , you may find the firmware in the installation folder as below:

pastedImage_1.png

To download the firmware, please refer to Program the firmware to PNEV5180B board for details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply