Building explore-nfc from source on Pi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building explore-nfc from source on Pi

1,393 Views
noelkendall
Contributor I

Can anyone outline the correct way to build the NFC Explorer software stack for Raspbian Jessie?

The documentation in AN11802.pdf does not result in a clean compile.

Two artifacts are available: SW3693.zip and SW282816.zip

The board I am using this with is NXP-EXPLORER 1.6.

Looking through the source code from SW3693.zip, I am not finding support for this board. I could be wrong, of course, but if I am right, I am wondering if the SW3693.zip version is incorrect for support for that board.

If it is incorrect, is there a link available to the correct version of SW3693.zip that does support the board?

Tags (1)
0 Kudos
Reply
0 Replies