Bal Driver Implementation and timing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bal Driver Implementation and timing

1,913 次查看
sandeepbettahal
Contributor I

Hi,

We are using PN5180 on Linux based custom board used for payment applications. 

Using example applications, we see that there are around 3 sec delay between some of the transactions.

We use Bal driver from https://github.com/NXPNFCLinux/nxprdlib-kernel-bal and SW3693-1 package from NXP as reader library.

One of the obvious problems I see with BAL driver is, it registers for only Falling edge of busy line.

status = request_threaded_irq(bal.busy_irq, bal_busy_isr,
NULL,
IRQF_TRIGGER_FALLING,
"bal", &bal);

For the first transaction, Bal_write will not wait for busy line and goes ahead and performs SPI write, but for next transaction, it will wait for 3 secs as the timeout for completion in bal_write is 3 secs. The only possible way to avoid this 3 seconds is, if data is fed continuously and PN5180 completes write/read transaction and brings down busy line in this 3 secs waiting time of next write/read.

Is this how it was designed?

Shouldn't driver hold the status of busy line by registering for both IRQF_TRIGGER_FALLING and IRQF_TRIGGER_RISING and read the busy line (as most likely it will be connected to GPIO) and keep track of busy line status. Go to wait in read/write only if busy line is high.

Regards,

Sandeep

标签 (2)
0 项奖励
回复
1 回复

1,686 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Sorry for the late response, by any chance have you checked the complete folder available with the API documentation? I believe you will find a lot of useful information about the BAL implementation and available APIs.

Beside it,  I will ask about it and if I get any response if it was designed that way, I'll update you. 

Regards, 

Estephania

0 项奖励
回复