Authentication Timeout [Mifare classic] [NP5180]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Authentication Timeout [Mifare classic] [NP5180]

2,578 Views
jaime_feller
Contributor I

My application uses 2 sets of keys, the routine usually checks if it can authenticate with the primary keys and if that fails go for the secondary keys, everything works okay, but the timeout of phalMfc_Sw_Authenticate is a bit to long (about 320 ms until I get the PH_ERR_IO_TIMEOUT), there is anyway to shorten this timeout?

thanks for your help

0 Kudos
Reply
2 Replies

2,414 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Jaime,

Would you please help to check address 0x12 in the EEPROM of PN5180 regarding the firmware version? Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,856 Views
SiMu
Contributor I

Hello,

is there a solution to this problem. I have exactly the same behavior as described above

0 Kudos
Reply