Activation error Cockpit v.2.3(PN5180)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Activation error Cockpit v.2.3(PN5180)

4,966件の閲覧回数
nakaiso
Contributor II

I could download SW3524 and install PN5180 NFC Cockpit v.2.3.

According to SW35234 page 17 to 18, I tried to activate MIFARE, and encounterd error at 3rd step(pressed the button(activate layer3).

What should I check?

 

errorlog.jpg

0 件の賞賛
返信
8 返答(返信)

4,665件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Could you please let us know the exact steps you are following after connecting the board? Also, please let us know which model of MIFARE products you are working with.

Thank you.

Regards,

Ivan.

0 件の賞賛
返信

4,665件の閲覧回数
nakaiso
Contributor II

Hi,

Thanks for your reply.

My experiment procedure is shown below.

1) launch the PN5180 NFC cockpit 2.3.

2) press [Load protocol] in TypeA tab

3) press [Field on]

4) press [activate layer3]

Then, error message appear in log monitor.

0 件の賞賛
返信

4,665件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Thank you for sharing the info. It was possible to activate a MIFARE Plus card with NFC Cockpit v4.8.0, please see below:

pastedImage_1.png

Could you please try with the latest version of NFC cockpit available so far?

Download link:

NFC Cockpit

Regards,

Ivan.

0 件の賞賛
返信

4,665件の閲覧回数
nakaiso
Contributor II

Hi,

Thanks for your reply.

According to your advise, I installed latest ver. of NFC cockpit(v.4.8.0, FW v4.0), and tried to activate the board.

My experiment procedure is shown below.

1) launch the PN5180 NFC cockpit 4.8.0

2) press [Load protocol] in TypeA tab

3) press [RF Field on]

4) press [Activate layer3] 

ERROR:RFProtocolTypeAService:RequestA Failed HAL,IO_TIMEOUT

additionally, press [Activate Layer4]

ERROR:RFProtocolTypeAService:ActivateCard() Failed HAL,IO_TIMEOUT

What should I check?

fig2.png

4,665件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

This problem seems to be on the Tag's side. By any chance, is the card on the eval board antenna when Layer 3 and Layer 4 are activated?

Could you please provide details about the Tag you are working with? -In my case, I am activating a MIFARE Plus X 2K both, on Layer 3 and 4, please see below:

pastedImage_1.png

In case you are not sure with Tag you are working with, please use our NFC TagInfo tool for Android. This could also help us to discard that the Tag is not functional.

Regards,

Ivan.

0 件の賞賛
返信

4,665件の閲覧回数
riley_baird
Contributor I

I will comment and mention that the NFC Tag Info by NXP (on iOS) is a completely useless app. It only shows NDEF data that exists on the card, and absolutely nothing about what type the card is. The screenshots on Android show it may be more useful? This app should be removed from the iOS store at this state, it doesn't help anyone.

0 件の賞賛
返信

4,665件の閲覧回数
nakaiso
Contributor II

Hello,

According to your advise, I could operate NFC cockpit by using Mifare DESFire card!

I had chosen wrong Tag, so NFC cockpit did not work well.

I appriciate your support!

0 件の賞賛
返信

4,665件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

I am glad I could help.

Have a nice day!

BR,

Ivan.

0 件の賞賛
返信