About NFC NXP Library (reader).

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About NFC NXP Library (reader).

1,635 次查看
moureton_etienn
Contributor I

     Hi, as a Python beginner, i have some questions about my project.

     Bought few times ago a NFC sensor : https://www.element14.com/community/docs/DOC-71574  that should work with my Raspberry Pi Zero W.

I'm programming on PyCharm on Windows 10 (yes, the library is for Linux, know it) before exporting it on the Pi. The problem is that i see on the "Library Guide" that the sensor only works with PI 2/3. So, i want to know if i can keep my Pi Zero or if it's impossible ?

     Thanks for the answer all.

标记 (5)
0 项奖励
回复
1 回复

1,467 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

There should be no hardware issue to use Zero W with the NFC sensor as Zero W has the same 40 pin interface definition, and AN11802 doesn't specify the platform version, so I think you may use Pi Zero with that board.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复