AN11597,PCBboard firmware code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN11597,PCBboard firmware code

4,123件の閲覧回数
annachen
Contributor I

I am testing the AN11597 ,and the board and the NTAG I2C DEMO works good,and i make my own pcbboard,in order to make it works,can you please provide the pcbboard firmware version of 1.6,please?

0 件の賞賛
返信
4 返答(返信)

3,817件の閲覧回数
annachen
Contributor I

And in what Build Environment is it worked,please

0 件の賞賛
返信

3,817件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello anna chen:

- If you have the NTAG I2C Demoboard (without LCD display) the firmware sources are in the next product page under Software & Tools:

NTAG I²C - Energy harvesting NFC Forum T|NXP

- In case you used the NTAG I2C plus explorer board (with onboard LCD display) the firmware is in the next page under Downloads:

NTAG I²C plus Explorer Kit|NXP

In either case the projects were developed with LPCXpresso IDE.

I hope this helps.

Regards!

Jorge Gonzalez

0 件の賞賛
返信

3,817件の閲覧回数
annachen
Contributor I

Dear Jorge Gonzalez:

I downloaded from the https://www.lpcware.com the latest version of v8.1.4,unfortunately it can't setup on my computer(windows xp),which version can work on the xp systems please?

0 件の賞賛
返信

3,817件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi anna chen:

Windows XP is no longer supported, but according to the next post in lpcware forum the last version of LPCXpresso IDE tested with Windows XP was 7.0.2:

Windows XP | www.LPCware.com

You can try that one. There is a list of downloads for Windows in the next link:

LPCXpresso IDE Windows Installer | www.LPCware.com

:smileyinfo: NOTE: I cannot guarantee that the NTAG I2C projects mentioned will work with that version of the IDE.

Regards!

Jorge Gonzalez

0 件の賞賛
返信