您好:
1.我想用PN7462AU的io口模拟串口(波特率是 115200)是否可行?
2.我测试了一下,一个io写高电平然后返回的时间为2.5us,写一个低电平然后返回的时间也是2.5us,能否有更快的速度,我测试过其他单片机的周期为330ns
3.读取一个io管脚的周期在3us左右,能够更快呢?
4.我把例程按照要求烧录到开发板里,然后按RST_N键,为什么不能运行?(我调试的时候又没有问题)
(我的开发板型号 : PNEV7462B V2.2)
5.我把历程phExRf用调试的方式测试,运行正常,但是我实际烧录进去却不行,请问是怎么回事,(我也有先运行user_ee.bat,在把得到的新的user_ee.bin烧录进去)可以以调试的方式烧录进去却没事。
this may help you
其实我想确认的是问题 1 2 3 ,我的设备需要一个usb,一个串口(115200),就是不知道怎样能实现这个功能。或者模拟的话如何模拟,能不能成功
Hello Xubin,
PN7462 can support HSUART and USB interface Simultaneously, see below, please!
So you don't need to emulate UART protocol by GPIO!
In addition, even if there is ARM - M0 core in PN7462, it is only NFC reader with M0 core, you couldn't compare it with MCU on GPIO performance.
Have a nice day!
Best Regards,
Weidong Sun
Only one interface is active at a time.