PN7160 - Extended NFC Factory Test Application for Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7160 - Extended NFC Factory Test Application for Linux

PN7160 - Extended NFC Factory Test Application for Linux

Extended NFC Factory Test Application includes: 

  • Get Current value (current measurement in mA)
  • DPC Check (Available from FW. Version 12.50.06)
  • Get AGC Value 
  • Get AGC Value NFCLD (AGC value reading with fixed NFC Level Detector level)
  • Dump EEPROM settings 
 
EEPROm_dump.png
How to get it: 
  1. Just download the app from Github.
  2. Replace the "NfcFactoryTestApp.c" with the file which is here in the attachment. 
  3. Run the application as described in ->AN13287.

 

Tomas Parizek 

Customer Application Support 

ラベル(1)
添付
コメント

Can you provide the Android version

7160芯片,android 14 ,NFC FW 12.50.09

使用getAGC时返回值不对,请问是什么问题 

 

mark_tang_0-1718936125259.png

 

Hello mark_tang, 

 

For Android, You should just extend the code in the same way as for Linux. Then it should work. 

 

About the AGC value, yes it is strange. You are getting quite a high value, let me double-check the AGC range. 

 

Thanks ! 

 

BR

Tomas 

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
水曜日
更新者: