OM27642 & TDAEV8035 - Quick Start Guide

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM27642 & TDAEV8035 - Quick Start Guide

OM27642 & TDAEV8035 - Quick Start Guide

The TDAEV8035 evaluation board is inserted into the connector slot located on the top side of the PN7642 EVK, as shown in the figure below.
 
Tomas_Parizek_0-1783430718849.png

 

Dedicated jumper settings are required to ensure proper connection and operation of the TDAEV8035 extension board.
 
  • J23 - Position 2-3
  • J65, J63, J64 - Closed 
  • J59 - Closed (Positions 1-2, 3-4, 5-6)
Once the jumpers are configured correctly, users can run the example applications provided in the PN7642 MCUXpresso SDK.
 
Tomas_Parizek_0-1783431007072.png

 

After building the example project, select the right card slot (TDA8035) on the board. By default, the SIM card slot (Slot 1) is used. To use the contact card slot instead, modify the slot selection in the following section of the code.
 
Tomas_Parizek_1-1783431121171.png

 

  • E_AUX_SLOT1 - SIM slot (default) 
  • E_AUX_SLOT2 - Contact card slot 

The selected card slot is indicated by a red LED.

  • D1 - SIM slot 
  • D2 - Contact Card slot
Once all required settings have been applied, the example application can be started and a contact card can be inserted into the selected card slot. 
 
The results can be viewed in the console.
 
Tomas_Parizek_0-1783431467282.png
无评分
版本历史
最后更新:
‎07-07-2026 06:42 AM
更新人: