996002_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

996002_en-US

996002_en-US

FXTHxx with IAR ?

Hello ,

I have a sensor called FXTH871511DT1CT-ND which can be programmed at the same time. I need to program this sensor and print the data. For this I use one J-Link and one MRB-KW019030JA. I can program MRB-KW019030JA with J-Link in the IAR program. Next, I need to program FXTH871511DT1CT-ND. My compiler does not have a FXTHxx library (in IAR). Do I have a chance to program this FXTHxx via MKW01xx ?  Please help me .

Re: FXTHxx with IAR ?

Hi Kerem,

Only CodeWarrior IDE compiler supports the FXTH, and only the P&E Micro Multilink tool supports the programming of the FXTH. The FXTH cannot use IAR and JLink.

The TPMS application team has developed the demo “LF RF Bootloader”, that can be downloaded from here, which implements wireless reprogramming of the FXTH (using LF and RF). However, this requires a portion of the FXTH memory to be previously programmed with the bootloader code. And this bootloader code can only be opened in CodeWarrior and programmed with the P&E Micro Multilink tool.


From this webpage, the  “Starter Package for FXTH and MKW01” can be downloaded. Inside the package are several folders containing demo code and documentation. Among them, the document “Installing and using CodeWarrior” gives information on how to download a free version of CodeWarrior IDE, and links to buy the P&E Micro Multilink tool.

Best regards,

Tomas

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-04-2026 08:25 AM
更新者: