984111_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

984111_en-US

984111_en-US

Get data from FXTH87 with FRDM-KW01 evaluation board without RF?

Hi, I'm new to MCU programming and I want to know if getting data from FXTH87 evaluation board with FRDM-KW019032 without RF is possible. If it is possible, is there a document that I can follow? How can I manage it? All of the examples are about getting the data with RF.

Ateş

Re: Get data from FXTH87 with FRDM-KW01 evaluation board without RF?

Hi Ateş,

The FXTH87 can transfer information to another MCU using software SPI or software IIC, as there is no hardware SPI or C block in the FXTH87.

There are several ways to trigger the Pressure/Temperature measurement and SPI/IIC transfer: for example, it can be triggered by a periodic wake up using the FXTH PWU block or by an external signal triggering an interrupt on a FXTH GPIO (using the KBI block of the FXTH87). However, currently there is no code example/document illustrating this available.

Best regards,

Tomas

标记 (1)
无评分
版本历史
最后更新:
‎02-04-2026 06:03 AM
更新人: