The NXP Sensor Fusion Toolbox has the Flash LPCXpresso Binary -> OM13070 LPC4337 in the menu
Is the source code of this version of the sensor fusion library available?
Hi Pavel,
As part of ISSDK enablement for NPIs like RT10xx (RT1050, RT1060, RT1064, RT1020), our Sensors software team signed up to provide sensor usage examples only as early enablement before their SDK launch. This is the reason that all MCU NPIs where ISSDK has been part of their MRD/PRD for early enablement, we provide ISSDK middleware support to deploy only sensor examples for a custom kit with FRDM-STBC-AGM01 (and not algorithm examples like sensor fusion and pedometer).
Best regards,
Tomas
Hi Tomas,
Thank you, downloaded the LPC54114 AGM01 SDK and it has all the ISSDK and Sensor Fusion library files.
I was also looking at the iMXRT1050 so I downloaded the iMXRT1050 with AGM01 SDK and it has the ISSDK and the sensor drivers but the \middleware\issdk\algorithms\sensorfusion\sources are missing from the SDK. Is there a reason why the sensorfusion/sources are missing from the iMXRT1050 SDK?
Thanks,
Pavel
Hi Pavel,
The binaries available as part of File -> Flash LPCXpresso Binary options in the NXP Sensor Fusion Toolbox were custom made for Sensor Fusion Toolbox v5 (older version) compatible with KSDK v1.2 using the Processor Expert module on Code Warrior toolchain (Kinetis SDK v1.2 is no more available). I do not have the source code or Code Warrior project for this binaries since latest Sensor Fusion Toolbox v7.x is integrated into ISSDK and is compatible with MCUXpresso SDK v2.5.0 (latest version). Even MCUXpresso SDK builder does not support the LPC families listed in the Sensor Fusion Toolbox File -> LPCXpresso Binary tab (i.e. LPC4337, LPC1549 and LPC11U68). The MCUXpresso SDK builder only supports LPC5xxxx and LPC8xxx series of MCUs:
So I would recommend to use these LPC MCU families supported by MCUXpresso SDK latest version (since support model will be sustainable) and the ISSDK based Sensor Fusion examples we have for the following LPCXpresso boards:
I hope it helps.
Best regards,
Tomas
PS: If this answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.