836106_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

836106_en-US

836106_en-US

6D Sensor Fusion Algorithm Problem

Hi all,

I did some tests with NXP Sensor Fusion Library on my custom hardware. The library works pretty well under most conditions. But when I move the board forward and backward in less than 1 sec - periodically to test the behaviour under vibration (especially the board in a diagonal position to the surface), sometimes I see abrupt changes at output. Please find attached the pictures. In the pictures, the blue line is output from NXP fusion library; the red line is output from a commercial inclinometer. The output from NXP lib. somewhat goes to a point  far away from real position. In other cases it tracks the red line closely. I tested my custom hardware with another algorithm to verify it; I had no problem with it.

I used NXP 6D Acc+Gyro algorithm for testing. The NXP lib fusion rate and sensor sampling rate is 200Hz. I also tried with 400Hz sampling rate but no change. May a software defect exist which cause incorrect output in the NXP Sensor Fusion algorithm?

SensorFusion
Tags (1)
No ratings
Version history
Last update:
‎02-04-2026 07:39 AM
Updated by: