818105_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

818105_en-US

818105_en-US

refresh policy problem S32K142 EVB

I open project from file system then get this warning.

How to Fix this warning????

Description Resource Path Location Type
In Debug_FLASH configuration the refresh policy S32K142_EVB_JumpStart_Firmware does not match the project name S32K142_EVB_JumpStart_Firmware S32K142_EVB_JumpStart_Firmware S32K142_EVB_JumpStart_Firmware Refresh Policy Problem. 123.PNG

Re: refresh policy problem S32K142 EVB

A few years to late but i can confirm that for me, doing the last step only then cleaning and compiled fixed it all.

I just got into the .cproject, searched all references to the old project name and changed them for the new project name. Then it compiled without these warnings. 

I guess removing the warnings does the same as cleaning. 

Re: refresh policy problem S32K142 EVB

Hello,

My colleague @BlackNight has an excellent blog on this topic. Please check it out for your solution!

MCU on Eclipse | Eclipse Project ‘Refresh Policy’: Broken Incremental Build with External Make?

Best regards,

Mike

Re: refresh policy problem S32K142 EVB

_0-1691407927034.png_0-1691407927034.pngFollowing the previous solution, I tried but did not solve the problem

Re: refresh policy problem S32K142 EVBpointless
Re: refresh policy problem S32K142 EVB

I had the same problem after I copied an existing build configuration in S32DS 2018.R1 and delete the configuration gain in S32DS.

The problem is that S32DS does not completely delete the reference to the configuration but only deletes its properties:

Working configuration:

<configuration configurationName="Release">
 <resource resourceType="PROJECT" workspacePath="/Project_Name"/>
configuration>‍‍‍‍‍‍

Deleted Configuration:

<configuration configurationName="Debug_Release"/>

So what I did to solve the warnings is:

  1. Right click and delete all warnings in the console after opening the project
  2. Close the project
  3. Delete the unused configuration tag shown above in the .cproject file located in the project root folder

This was of course after I had already deleted the built configuration in S32DS itself.

Re: refresh policy problem S32K142 EVB

As you say Xu zhao, this issue is not resolved in S32 Studio.

When you duplicate a project S32 Studio fails to rename certain files and configurations.

You have to review all Debug Configurations for your project (right click on project > Debug As > Debug Configuration)

You will also have to review the Refresh Policy in each of your C/C++ Build configurations. Delete the wrong resources and add the proper ones

RefreshPolicy.PNG

Re: refresh policy problem S32K142 EVB

hi, my IDE is

S32 Design Studio for ARM

Version: 2018.R1
Build id: 180815

also have this bad problem. always warning in problem console.

I had check the prj names, it is sure correct.

still not solved....

Re: refresh policy problem S32K142 EVB

fix by S32DS ARM 2.0 version. thanks~

Re: refresh policy problem S32K142 EVB

Hi, 

there are different names for .launch xml files - located in project root -> Project_Settings\Debugger. Just rename these files  to met the project name:

pastedImage_1.png 

On screenshot I already renamed the first two files. In my case there was extra _OOBE_ in filename. 

Hope it helps. 

Jiri 

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 11:51 PM
更新者: