811353_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

811353_en-US

811353_en-US

Sensor MPX5700ASX ¿liquid/wine?

Hi.

I would like to know if the #MPX5700ASX sensor can be used for #liquids and can be in contact with food (Food Security Law).

If this #sensor can not be used for this, do you know any other model that does work?

Thanks

Re: Sensor MPX5700ASX ¿liquid/wine?

Ok, 

thanks!

Re: Sensor MPX5700ASX ¿liquid/wine?

Hi Fran,

We do not recommend direct contact with any kind of liquid substances. The sensing die is covered with a protective gel, this gel might crack or get washed out and with this changing the characterization of the device, therefore we do not recommend it for any of NXP pressure sensors.


However, as you may know, our products are used in washing machine applications, which would expose the gel to a humid environment. In such applications, the device is located at the top of a measurement tube - so water level is indirectly measured through the water pushing a trapped air column up to the sensor. As you can see, the sensor does not have direct contact with water, but is separated by the air column.


For more information, please refer to the AN3728.

Best regards,

Tomas

Tags (1)
No ratings
Version history
Last update:
‎02-04-2026 10:04 AM
Updated by: