Hello:
The program doesn't run after reset after downloading the code, it should be downloaded to RAM, how to configure the project to download to Flash.
Thanks Robin,
我已经帮宁工确认了Flashloader的下载算法没有问题,同时,确认Link文件指定的中断向量地址也没问题,附上截图,请您帮忙看一下,多谢。
Hi, Robin.
Jack's problem is really my problem.
I'm using a KEAZN64 chip, developed in IAR 8.30.1, based on the KEA64 routines.
Plugging in the emulator to download and debug the program works fine.
After generating the .out file and downloading the file and unplugging the emulator, the program doesn't run properly, it feels like the program is burned into ram but not into flash.
Configuration options - >linker - > config - > KEAZN64xxx2.icf
How to configure options or other configurations?
Hello, Jack.
It's not clear which routine you're using.
If it is the TRK-KEA128_IAR_LABTS1 example downloaded from the TRK-KEA128: Kinetis KEA128 StarterTRAK for CAN Applications page of the... program to set it up.
Best Regards.
Robin.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------